0611IB1302-08

Energy Measurements

General Description

The energy measurements are refreshed every second. Energy measurements are saved every hour in the non-volatile memory of the MicroLogic trip unit.

Energy measurements include:

  • active energy Ep

  • reactive energy Eq

  • apparent energy Es

  • active energy counted positively (EpIn) or negatively (EpOut), according to the configuration of register 3316 Power Flow Sign.

  • reactive energy counted positively (EqIn) or negatively (EqOut), according to the configuration of register 3316 Power Flow Sign.

  • active energy and reactive energy are accumulated according to the configuration of register 3324 (absolute mode by factory setting) Energy Accumulation Mode.

The reset minimum/maximum command (command code = 46728) can reset the content of the energy measurement registers, cumulative energy measurements excepted.

NOTE: The power flow sign configuration command (command code =47240) can reset the content of the energy measurement registers excluding the cumulative energy measurements.

Energy Registers

Energies are stored in big-endian format: the most significant word is transmitted first and the least significant second.

Examples

If Ep = 7589 kWh, then:

  • register 2000 = 0 (0x0000)

  • register 2001 = 7589 (0x1DA5)

If Ep = 4,589,625 kWh, then:

  • register 2000 = 70 (0x0046)

  • register 2001 = 2105 (0x0839)

4589625 = 70x65536 + 2105

Address

Register

RW

X

Unit

Type

Range

A/E

Description

0x07CF–

0x07D0

2000–

2001

R

1

kWh

INT32

-1 999 999 999–+1 999 999 999

E

Active energy: Ep

0x07D3–

0x07D4–

2004–

2005

R

1

kVARh

INT32

-1 999 999 999–+1 999 999 999

E

Reactive energy: Eq

0x07D7–

0x07D8

2008–

2009

R

1

kWh

INT32

0–1 999 999 999

E

Active energy counted positively: EpIn

0x07DB–

0x07DC

2012–

2013

R

1

kWh

INT32

0–1 999 999 999

E

Active energy counted negatively: EpOut

0x07DF–

0x07E0

2016–

2017

R

1

kVARh

INT32

0–1 999 999 999

E

Reactive energy counted positively: EqIn

0x07E3–

0x07E4

2020–

2021

R

1

kVARh

INT32

0–1 999 999 999

E

Reactive energy counted negatively: EqOut

0x07E7–

0x07E8

2024–

2025

R

1

kVAh

INT32

0–1 999 999 999

E

Apparent energy: Es

0x07EB–

0x07EC

2028–

2029

R

1

kWh

INT32

0–1 999 999 999

E

Cumulative active energy counted positively (cannot be reset): EpIn

0x07ED–

0x07EE

2030–

2031

R

1

kWh

INT32

0–1 999 999 999

E

Cumulative active energy counted negatively (cannot be reset): EpOut