0611IB1302-08

Alarm Status

Addresses and Registers List

The following table describes the alarm status addresses, and registers regarding the IO module.

IO Module

Addresses

Registers

IO 1

0x3989–0x39A6

14730–14759

IO 2

0x4541–0x455E

17730–17759

Generic Alarm Status for IO 1

@ Justine > Define and rename ULP and TI086 formats of the IO module event history

The order and the description of the generic alarm status registers for IO 2 are the same as those of IO 1.

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3989

14730

R

INT16U

Quality of each bit of register 14731:

  • 0 = Invalid

  • 1 = Valid

0x398A

14731

R

INT16U

IO module history format register

0

ULP format

1

TI086 format

2–15

Reserved

0x398B

14732

R

INT16U

Quality of each bit of register 14733:

  • 0 = Invalid

  • 1 = Valid

0x398C

14733

R

INT16U

IO module command type

Factory setting = 3, both write command mechanisms are enabled.

0

1 = Complex commands

1

1 = Simple commands

Simple commands can be disabled by sending a command

2–15

Reserved

0x398D–0x3992

14734–14739

Reserved

0x3993

14740

R

INT16U

Quality of each bit of register 14741:

  • 0 = Invalid

  • 1 = Valid

0x3994

14741

R

INT16U

IO module generic alarm 1 status register.

0

IO module in STOP mode: IO module is not working and must be replaced.

1

IO module in ERROR mode: IO module is working in degraded mode.

2

Threshold overrun on I1 counter

3

Threshold overrun on I2 counter

4

Threshold overrun on I3 counter

5

Threshold overrun on I4 counter

6

Threshold overrun on I5 counter

7

Threshold overrun on I6 counter

8

Threshold overrun on O1 counter

9

Threshold overrun on O2 counter

10

Threshold overrun on O3 counter

11

Switchboard temperature threshold 1 overrun

12

Switchboard temperature threshold 2 overrun

13

Switchboard temperature threshold 3 overrun

14–15

Reserved

0x3995

14742

R

INT16U

Quality of each bit of register 14743:

  • 0 = Invalid

  • 1 = Valid

0x3996

14743

R

INT16U

IO module generic alarm 2 status register.

0

User-defined input 1 alarm

1

User-defined input 2 alarm

2

User-defined input 3 alarm

3

User-defined input 4 alarm

4

User-defined input 5 alarm

5

User-defined input 6 alarm

6–15

Reserved

Cradle and Drawer Management Alarms for IO 1

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3997

14744

R

INT16U

Quality of each bit of register 14745:

  • 0 = Invalid

  • 1 = Valid

0x3998

14745

R

INT16U

Cradle management alarms register

0

Cradle position discrepancy

1

Disconnection of the circuit breaker from cradle is overdue.

2

Cradle has reached its maximum number of operation

3

Remaining service life of cradle is below alarm threshold

4

New MicroLogic control unit has been detected

5–7

Reserved

8

Drawer position discrepancy

9–15

Reserved

Motor Alarms for IO 1

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3999

14746

R

INT16U

Quality of each bit of register 14747:

  • 0 = Invalid

  • 1 = Valid

0x399A

14747

R

INT16U

IO motor alarms

0–15

Reserved

Miscellaneous Application Alarms for IO 1

Address

Register

RW

Unit

Type

Range

Bit

Description

0x399B

14748

R

INT16U

Quality of each bit of register 14749:

  • 0 = Invalid

  • 1 = Valid

0x399C

14749

R

INT16U

Other application alarms register

0

Auxiliary contact of load contactor 1 is not closed.

1

Auxiliary contact of load contactor 1 is not opened.

2

 

3

Reserved

4–15

Reserved

0x399D

14750

R

INT16U

Quality of each bit of register 14751:

  • 0 = Invalid

  • 1 = Valid

0x399E

14751

R

INT16U

Predefined input alarms register

0

Earth-leakage trip signal contact (SDV)

1

Control voltage presence contact

2

Surge protection status contact

3

Surge failure contact

4

Switch-disconnector ON/OFF indication contact (OF)

5

Fuse blown indication contact

6

Emergency stop

7

Switchboard temperature contact

8

Switchboard ventilation contact

9

Switchboard door contact

10–15

Reserved

0x399F

14752

R

INT16U

Quality of each bit of register 14753:

  • 0 = Invalid

  • 1 = Valid

0x39A0

14753

R

INT16U

IO module discrepancy alarms register

0

Critical hardware discrepancy

1

Critical firmware discrepancy

2

Non-critical hardware discrepancy

3

Non-critical firmware discrepancy

4–15

Reserved

0x39A1–0x39A6

14754–14759

Reserved