Event Commands
Acknowledge a Latched Output
The user can read the SDx module outputs parameters from register 9801 to 9810 Configuration of the SDx Module.
To acknowledge a latched output, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
46216 |
A/E |
Command code = 46216 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
12 |
A/E |
Number of parameters (bytes) = 12 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
A/E |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
A/E |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
A/E |
Password of the command: Administrator or Operator user profile password |
|
0x1F45 |
8006 |
– |
– |
INT16U |
1–2 |
A/E |
1 = relay 1, 2 = relay 2 |
Acknowledge a Trip
To acknowledge a trip, the user must set up the command registers the following way:
|
Address |
Register |
X |
Unit |
Type |
Range |
A/E |
Description |
|---|---|---|---|---|---|---|---|
|
0x1F3F |
8000 |
– |
– |
INT16U |
46217 |
A/E |
Command code = 46217 |
|
0x1F40 |
8001 |
– |
– |
INT16U |
10 |
A/E |
Number of parameters (bytes) = 10 |
|
0x1F41 |
8002 |
– |
– |
INT16U |
5121 |
A/E |
Destination = 5121 (0x1401) |
|
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
A/E |
Security type of the command |
|
0x1F43– 0x1F44 |
8004– 8005 |
– |
– |
OCTET STRING |
– |
A/E |
Password of the command: Administrator user profile password |