0611IB1302-08

Intelligent Modular Unit

Definition

FYI, this map is shared with EIFE, IFE, FDM121, IO Module, MTZ Modbus guide, NT/NW Modbus guide, and NSX Modbus guide.

A modular unit is a mechanical and electrical assembly containing one or more products to perform a function in a switchboard (incoming protection, motor command, and control).

The circuit breaker with its internal communicating components (MicroLogic control unit or MicroLogic trip unit) and external ULP modules (IO module) connected to one communication interface is called an intelligent modular unit (IMU).

An IMU is composed around a circuit breaker from the following ranges:

  • MasterPact MTZ circuit breakers

  • MasterPact NT/NW circuit breakers

  • ComPacT NS 630b–1600 circuit breakers

  • ComPacT NS 1600b–3200 circuit breakers

  • PowerPacT P- and R- frame circuit breakers

  • ComPacT NSX circuit breakers

  • PowerPacT H-,J-, and L- frame circuit breakers

ULP Modules Per Circuit Breaker Range

The following table lists the compatible ULP modules for each range of circuit breakers.

ULP Module

Part Number

MasterPact MTZ with ULP Port Module and MicroLogic Control Unit

MasterPact NT/NW or ComPacT NS or PowePacT P- and R-Frame with BCM ULP Module and MicroLogic Trip Unit

ComPacT NSX or PowerPacT H-, J-, and L-Frame with BSCM Module and/or MicroLogic Trip Unit

IFE Ethernet interface for one circuit breaker

LV434001

LV434010

IFE Ethernet switchboard server

LV434002

LV434011

EIFE Embedded Ethernet interface for one MasterPact MTZ drawout circuit breaker

LV851001

Spare part kit EIFE for one MasterPact MTZ1 drawout circuit breaker

LV851100SP

Spare part kit EIFE for one MasterPact MTZ2/MTZ3 drawout circuit breaker

LV851200SP

IFM Modbus-SL interface for one circuit breaker

TRV00210

STRV00210

IFM Modbus-SL interface for one circuit breaker

LV434000

FDM121 front display module for one circuit breaker

TRV00121

STRV00121

IO input/output application module for one circuit breaker

LV434063

USB maintenance interface

TRV00911

STRV00911

For more information on the ULP System and its components, refer to DOCA0093EN ULP (Universal Logic Plug) System for ComPact and MasterPact Circuit Breakers – User Guide.

Communication Architecture

A

FDM128 Ethernet display for eight devices

B

FDM121 front display module for one circuit breaker

C

IFE Ethernet interface for one circuit breaker

D

IFE Ethernet switchboard server

E

IFM Modbus-SL interface for one circuit breaker

F

IO input/output application module for one circuit breaker

G

MasterPact MTZ1 or MTZ2/MTZ3 drawout circuit breaker

H

MasterPact MTZ1 or MTZ2/MTZ3 fixed circuit breaker

I

MasterPact NT/NW circuit breaker

J

ComPacT NS/PowerPacT M-,P,- and R-frame circuit breaker

K

ComPacT NSX/PowerPacT H-, J-, and L-Frame circuit breaker

L

ULP port module

M

EIFE Embedded Ethernet Interface for one MasterPact MTZ drawout circuit breaker

N

ULP line termination

O

RJ45 ULP cord

P

Circuit breaker BCM ULP cord

Q

NSX cord

Remote Controller

A remote controller is a device that is able to communicate with an IMU using a communication interface, such as the IFE Ethernet interface. For example, FDM128 Ethernet display for eight devices, supervisor, PLC, BMS, SCADA system, and so on, are remote controllers.

For the description of Modbus registers and commands, refer to the Modbus Communication Guides.