0611IB1302-08

List of MicroLogic Trip Unit Commands and Error Codes

List of Commands

The following table lists the available MicroLogic trip unit commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly Executing a Command.

Command

Command code

User profile

Long-time protection Long-Time Protection

45192

Administrator

Short-time protection Short-Time Protection

45193

Administrator

Instantaneous protection Instantaneous Protection

45194

Administrator

Ground-fault protection Ground-Fault Protection

45195

Administrator

Neutral protection Neutral Protection

45197

Administrator

Jam protection Jam Protection

45448

Administrator

Underload protection Underload Protection

45449

Administrator

Unbalance protection Unbalance Protection

45450

Administrator

Long-start protection Long-Start Protection

45451

Administrator

Acknowledge a latched output Acknowledge a Latched Output

46216

Administrator or Operator

Acknowledge a trip Acknowledge a Trip

46217

Administrator

Set up ENVT presence Set Up ENVT Presence

46472

Administrator

Reset minimum/maximum Reset Minimum/Maximum

46728

Administrator or Operator

Start/stop synchronization Start/Stop Synchronization

46729

Administrator or Operator

Power flow sign configuration Power Flow Sign Configuration

47240

Administrator

Power factor sign configuration Power Factor Sign Configuration

47241

Administrator

Energy accumulation mode configuration Energy Accumulation Mode Configuration

47242

Administrator

Current demand configuration Current Demand Configuration

47243

Administrator

Power demand configuration Power Demand Configuration

47244

Administrator

Set up nominal voltage Vn display Set Up Nominal Voltage Vn Display

47245

Administrator

Error Codes

Error codes generated by MicroLogic trip units are the generic error codes Result of the Command.