DOCA0257EN-01

AO Settings

Description

The TeSys Tera system supports up to two analog outputs (AO) with two LTMTAN21 expansion modules.

Parameter Setting

Each AO Settings function has the following configurable settings:

Parameter

Setting range

Default value

AO1 Source

  • None

  • L1 RMS Current

  • L2 RMS Current

  • L3 RMS Current

  • Average Current

  • L1–L2 RMS Voltage

  • L2–L3 RMS Voltage

  • L3–L1 RMS Voltage

  • Average Voltage

  • System Frequency

  • Total Active Power

  • Total Apparent Power

None

Analog Output Source Settings

The table lists the minimum and maximum setting values for each analog output source.

Analog Output source

Default Value

AO1 source minimum range

AO1 source maximum range

None

None

0

0

L1 RMS current

10 %FLC1

10 %FLC1

1000 %FLC1

L2 RMS current

10 %FLC1

10 %FLC1

1000 %FLC1

L3 RMS current

10 %FLC1

10 %FLC1

1000 %FLC1

Average current

10 %FLC1

10 %FLC1

1000 %FLC1

L1-L2 RMS voltage

20 %Vn

20 %Vn

150 %Vn

L2-L3 RMS voltage

20 %Vn

20 %Vn

150 %Vn

L3-L1 RMS voltage

20 %Vn

20 %Vn

150 %Vn

Average voltage

20 %Vn

20 %Vn

150 %Vn

System frequency

50 %NominalHz

50 %NominalHz

150 %NominalHz

Total active power

20 %Pn

20 %Pn

1000 %Pn

Total apparent power   

20 %Pn

20 %Pn

1000 %Pn

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.