DOCA0257EN-01

Overload

Description

In Overload starter, only two digital output is required for motor RUN command (CONTACTOR OUTPUT 1 (DO1) and Trip status (DO3)).

Wiring Diagram

Example of wiring diagram of the TeSys Tera system in Overload starter:

NOTE: Terminal O1 and O3 are connected in series.

Operating Principle

When Overload starter is selected, TeSys Tera system do not accept any start or stop command to control the motor. Start and stop has to be connected externally as shown in wiring diagram. In Overload mode, TeSys Tera system trips the motor on the occurrence of trip condition.

CONTACTOR OUTPUT 1 can be configured to any of the DO of TeSys Tera system. This enables the Maximum start per hour and the Anti-backspin timer functions in overload mode.

TeSys Tera system activates the CONTACTOR OUTPUT 1, if the motor is ready to start (that is no inhibit cause detected).

TeSys Tera system deactivates CONTACTOR OUTPUT 1, if any of the following motor stop cause is detected:

Combination of DO1 and DO3 will drive the motor.

DI/DO Default Assignment

When Overload starter type is selected, the default assignment and settings of digital inputs and digital outputs are as follows.

DI parameters

DI1 settings

DI2 settings

DI3 settings

DI4 settings

Trigger type

Active high

Active high

Active high

Active high

Input source

None

None

None

None

Validation time

10 ms

10 ms

10 ms

10 ms

DO parameters

DO1 settings

DO2 settings

DO3 settings

Active type

Active high

Active high

Active low

Input source

CONTACTOR OUTPUT 1

None

Trip status

Tag

Other

Other

Trip DO

Output type

Level

Level

Level

Pulse time

0 ms

0 ms

0 ms

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.