DOCA0257EN-01

LTMTCT/LTMTCTV Sensor Module

The LTMTCT/LTMTCTV sensor module measures the electrical parameters of a motor:

  • LTMTCT sensor module measures the motor currents.

  • LTMTCTV sensor module measures the motor currents and voltages.

LTMTCT/LTMTCTVT Horizontal Sensor Module

A Window for phase 1 current measurement
B Window for phase 2 current measurement
C Window for phase 3 current measurement
D

Phase voltage input connector (on LTMTCTV modules only)

E

Ground current measurement input connector

LTMTCTV Horizontal Sensor Module for SIDE Connector Applications

A

Phase voltage input connector

B

Window for phase 1 current measurement

C

Window for phase 2 current measurement

D

Window for phase 3 current measurement

E

Ground current measurement input connector

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.