DOCA0257EN-01

Block Output

Description

The Block Output function gives indication to upstream relays to block the trip, if one of the following protection functions detects a trip:

  • Short time over-current protection

  • Calculated ground trip protection

  • Measured ground trip protection

If TeSys Tera system detects pickup of any of the above mentioned protection, TeSys Tera system Block Output will be active which can be configured to digital output to inform upstream relays. Once TeSys Tera system issues trip for any of the above mentioned protection, the Block Output will be deactivated after the Contactor/Breaker Open Time set.

Parameters Settings

The Block Output function has the following configurable settings:

Parameter

Setting range

Default Value

Function

  • Disable

  • Enable

Disable

Contactor/Breaker Open Time

0.00–600.00 s in step of 0.01 s

0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.