DOCA0257EN-01

Phase Under Current

Description

The Phase Under Current condition generally occurs when motor is running with no load.

The Phase Under Current protection function generates the following signals:

  • Alarm: Any of the three-phase currents of the motor goes below the alarm level.

  • Trip: Any of the three-phase currents of the motor goes below the trip level for the specified time delay.

Parameter Setting

The Phase Under Current protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Alarm

Trip Level

15–100% of IFLC in step of 1%

50% of IFLC

Time Delay

0.1–6000.0 s in step of 0.1 s

10 s

Alarm Level

15–100% of IFLC in step of 1%

50% of IFLC

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

Auto

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

5 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.