DOCA0257EN-01

System Self-Diagnostic

Description

The LTMT main unit carries out a series of self tests to monitor:

  • Correct internal functioning of the LTMT main unit.

  • Correct functioning of the modules connected to the LTMT main unit.

  • Communication with the modules connected to the LTMT main unit.

The device internal error detected by the self tests are accessible from the LTMT main unit using the following interfaces:

  • A PC running SoMove FDT container software with TeSys Tera DTM installed and equipped with standard web server capability.

  • The LTMTCUF control operator unit.

  • A PLC or DCS through the communication network.

The last 20 detected device internal error detected are recorded by the LTMT main unit. Refer to Device Internal Records.

In case of device internal error detected, refer to the troubleshooting part in the TeSys Tera Motor Management System Installation Guide – DOCA0356EN.

Device Internal Error Detected

The motor or heater is stopped or inhibited by the motor starter logic when the following device internal error detected:

  • Sensor module communication error detected.

  • LTMT expansion module communication error detected.

  • Error detected during LTMT expansion module initialization.

  • Configuration error detected.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.