DOCA0257EN-01

Current Phase Reversal

Description

The Current Phase Reversal protection function helps to identify the wrong wiring of three-phase motor.

The Current Phase Reversal protection function generates the following signals:

  • Alarm: If the detected current phase sequence is not matching with the phase rotation setting .

  • Trip: If the detected current phase sequence is not matching with the phase rotation setting, for the specified time delay.

NOTE: Current Phase Reversal is not applicable in single-phase mode.

Parameter Setting

The Current Phase Reversal protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Alarm + Trip
  • Trip

Trip

Time Delay

0.1–6000.0 s in step of 0.1 s

0.1 s

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.