DOCA0257EN-01

Test Functions

If a device was tested in free air, the information will note that the device is not evaluated for use in an individual enclosure.

Self Test Without Trip

WARNING
UNINTENDED EQUIPMENT OPERATION
If the motor is connected to the contactor then there will be possibility of starting the motor for few seconds.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Press Test/Reset button for 3 to 15 s to perform a self test without trip. When the button is released, the LTMT main unit LED will turn ON in pattern 1 for 1 s. After 1 s, the LTMT main unit LED will turn ON in pattern 2 for 1 s. After 2 s from the beginning of the test, LTMT main unit comes out of the test mode.

LEDs

Pattern 1 LED status

Pattern 2 LED status

Device

Communication

NS

Motor Status

Trip/Alarm

The graphical representation of self test mode without trip is shown below:

A

Self test mode without trip

B

Reset button

C

LEDs

D

Pattern1

E

Pattern2

Self Test With Trip (If Motor is Stopped)

WARNING
UNINTENDED EQUIPMENT OPERATION
If the motor is connected to the contactor then there will be possibility of starting the motor for few seconds.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

When a self test with trip command is received from LTMTCUF control operator unit, communication network or a digital input of the LTMT main unit:

  • The LTMT main unit LED will turn on in pattern 1 for 1 s. After 1 s, the LTMT main unit LEDs will turn on in pattern 2 for 1 s.

  • The state of the trip digital output changes for 2 s.

  • After 2 s from the beginning of the test, the LTMT main unit comes out of the test mode, and the state of the trip digital output will change.

LEDs

Pattern 1 LED status

Pattern 2 LED status

Device

Communication

NS

Motor Status

Trip/Alarm

The graphical representation of self test mode with trip is shown below:

A

Self test mode with trip

B

Reset button

C

LEDs

D

Pattern1

E

Pattern2

Logic Test Mode

WARNING
UNEXPECTED BEHAVIOUR OF EQUIPMENT
The motor may turn on for few milli seconds before the TeSys Tera system trips while operating in Logic Test Mode.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The logic test function of the LTMT main unit can be used during commissioning of the motor. This function helps to check the wiring of the motor with LTMT main unit. Any one of the digital input of the LTMT main unit should be configured as logic test DI. The LTMT main unit enters into or exits from the logic test mode depending on the status of the logic test DI.

In logic test mode, the LTMT main unit allows you to start or stop the motor (contactors) to verify the wiring and bypass the following inhibit conditions:

  • Thermal memory inhibit

  • Max start inhibit

  • Low voltage inhibit

  • No voltage inhibit

In logic test mode, the LTMT main unit allows to reset the trip or auto resets the trip.

The LTMT main unit exits from the logic test mode in the following case:

  • Voltage detected by LTMTCTV sensor module.

  • Current detected by LTMTCT/LTMTCTV sensor module.

  • Logic test DI status is OFF.

The logic test mode can be set up using following interfaces:

  • A PC running SoMove FDT container software with TeSys Tera DTM installed and equipped with standard web server capability

  • The LTMTCUF control operator unit.

  • A PLC or DCS through the communication network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.