DOCA0257EN-01

Normal Inverse Overcurrent

Description

The TeSys Tera system provides the Normal Inverse Overcurrent (IEC class A – Standard inverse) protection function.

The trip time of the Normal Inverse Overcurrent protection is given by the formula:

Where:

  • T = Trip time

  • TMS = Time multiplier

  • k and α are the curve type constant. For standard inverse curve, k = 0.140 and α = 0.020

  • I = Actual current

  • Ip= Pick up current setting

The Normal Inverse Overcurrent protection function generates the following signals:

  • Alarm: Any of the three-phase currents of the motor goes above the alarm level.

  • Trip: Any of the three-phase currents of the motor goes above the trip level for the time derived from IEC class A curve and time delay (TMS) setting.

Parameter Setting

The Normal Inverse Overcurrent protection function has the following configurable settings:

Parameter

Setting range

Default value

Function

  • Disable

  • Alarm
  • Trip
  • Alarm + Trip

Disable

Trip Level

20–1000% of IFLC in step of 1%

50% of IFLC

Time Delay (TMS)

0.1–20.0 s in step of 0.1 s

0.1 s

Alarm Level

20–1000% of IFLC in step of 1%

50% of IFLC

Reset Mode

  • Reset key

  • DI

  • Communication

  • Auto

DI + Reset Key

Auto-Reset Delay (applicable only if Reset mode is Auto)

0.0–6000.0 s in step of 0.1 s

0 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.