DOCA0257EN-01

Direct Online

Description

The Direct Online starter requires the following digital inputs and outputs:

  • Two digital inputs for motor local start and local stop.

  • One digital output for motor RUN command CONTACTOR OUTPUT 1.

Wiring Diagram

Example of wiring diagram of the TeSys Tera system in Direct Online mode:

KM1: CONTACTOR OUTPUT 1

Logical Diagram

The following diagram shows the logical diagram of Direct Online starter.

Operating Principle

When Direct Online mode is selected, motor start is possible from one of the following sources:

If a start command is received from either of the above source and if the motor is Ready to Start (that is no inhibit cause detected), then TeSys Tera system activates the CONTACTOR OUTPUT 1.

TeSys Tera system deactivates CONTACTOR OUTPUT 1, if any of the following motor stop cause is detected:

DI/DO Default Assignment

When Direct Online starter type is selected, the default assignment and settings of digital inputs and digital outputs are as follows:

DI parameters

DI01 settings

DI02 settings

DI03 settings

DI04 settings

Trigger type

Active high

Active low

Active high

Active high

Input source

Local-START> DI

Local-STOP DI

Other

Mode Selection 1

Validation time

10 ms

10 ms

10 ms

10 ms

DO parameters

DO01 settings

DO02 settings

DO03 settings

Active type

Active high

Active high

Active high

Input source

CONTACTOR OUTPUT 1

Alarm Status

Trip Status

Tag

CNTR OP 1

Alarm DO

Trip DO

Output type

Level

Level

Level

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.