DOCA0093EN-05

RJ45 Plug/Plug ULP Cord Characteristics

Characteristics

The common characteristics of ULP cords are as follows:

  • Shielded cable with four twisted-pairs, 0.15 mm2 (26 AWG) cross-section, with typical impedance of 100 Ω

  • Shielded RJ45 plug connector at both ends, cable shielding connected to the connector cover (connector conforming to standard IEC 60603-7-1)

  • Color and order of internal wires conforming to standard EIA/TIA568B.2 (refer to RJ45 pin connection)

  • Insulation voltage of the outer sheath: 300 V (1)

  • Bending radius: 50 mm (1.97 in) (1)

(1) Cable must be compliant with installation requirements for voltage and temperature ratings. It is the responsibility of the user to select the correct cable for the specific installation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?