Composition Rules for Intelligent Modular Units (IMUs)
Introduction
Connection of an IMU in the ULP system is simple, but must comply with the rules concerning composition, RJ45 plug/plug ULP cords, and the ULP module power supply.
General Rule: Composition of an IMU
An IMU is composed of the following two device types:
-
One main device (circuit breaker or switch-disconnector ) and an internal ULP communication module
-
One or several external ULP modules
|
Main device type |
ULP modules |
|---|---|
|
|
|
|
|
MasterPact MTZ drawout circuit breaker with ULP port module |
|
|
MasterPact MTZ fixed circuit breaker with ULP port module |
|
|
(1) One IFE server with stacked IFM interfaces:
|
|
|
A |
ComPacT NSX , ComPacT NS , or MasterPact NT/NW circuit breaker |
|
B |
MasterPact MTZ circuit breaker with ULP port module |
|
C |
MasterPact MTZ drawout circuit breaker with ULP port module and EIFE interface |
General Rule: Order of ULP Modules in an IMU
Connect the ULP modules in a single IMU in any order. Base the connection on the ULP cable recommendations and the desired layout
for the ULP modules in the electrical equipment.
|
A |
ComPacT NSX , ComPacT NS , MasterPact NT/NW , or MasterPact MTZ circuit breaker |
General Rule: ULP Line Termination
The ULP modules placed at the end of the ULP line must have a ULP line termination (part number TRV00880) on the unused ULP RJ45 connector.
Example of ULP line termination on IFE interface:
Place the ULP modules which have an internal ULP line termination at the end of the ULP line, that is:
-
BSCM module or MicroLogic 5, 6, or 7 trip unit for ComPacT NSX circuit breakers.
-
BSCM module for ComPacT NSX DC circuit breakers.
-
BCM ULP module for ComPacT NS or MasterPact NT/NW circuit breakers.
-
ULP port module for MasterPact MTZ circuit breakers.
General Rule: Cables to Interconnect IMUs on Communication Networks
Do not connect the IMUs to one another with ULP cords.
-
Use only the Ethernet cable to interconnect IMUs connected to an Ethernet network.
A
ComPacT NSX , ComPacT NS , MasterPact NT/NW , or MasterPact MTZ circuit breaker
-
Use only the Modbus cable or stacking accessory to interconnect IMUs connected to a Modbus network.
A
ComPacT NSX , ComPacT NS , MasterPact NT/NW , or MasterPact MTZ circuit breaker
General Rule: Limitation of Number of MasterPact MTZ and ComPacT NSX Circuit Breakers
In case of floating power supply and when no IFM interface with part number TRV00210 is installed in the ULP system, the number of MasterPact MTZ and ComPacT NSX circuit breakers is limited by earth leakage currents as described in the following tables.
The limitation is valid for all MasterPact MTZ and ComPacT NSX circuit breakers used with a ULP connection.
Limiting the maximum number of IMUs on the same external DC power supply limits the cumulated leakage currents under 0.5 mA (human sensitivity level) or 3.5 mA (class I equipment).
Number of MicroLogic trip units or control units in the case of 0.5 mA leakage current maximum:
|
Ue (V L-N / U L-L) (Vac) |
Maximum number of MicroLogic X control units without VPS power supply ( MasterPact MTZ circuit breakers) |
Maximum number of MicroLogic X control units with VPS power supply ( MasterPact MTZ circuit breakers) |
Maximum number of MicroLogic trip units (ComPacT NSX circuit breakers) |
|---|---|---|---|
|
66 / 115 |
144 |
23 |
66 |
|
127 / 220 |
75 |
12 |
34 |
|
230 / 400 |
41 |
6 |
19 |
|
347 / 600 |
27 |
4 |
12 |
|
400 / 690 |
24 |
9 |
11 |
|
1,000 |
16 |
6 |
0 |
Number of MicroLogic trip units or control units in the case of 3.5 mA leakage current maximum:
|
Ue (V L-N / U L-L) (Vac) |
Maximum number of MicroLogic X control units without VPS power supply ( MasterPact MTZ circuit breakers) |
Maximum number of MicroLogic X control units with VPS power supply ( MasterPact MTZ circuit breakers) |
Maximum number of MicroLogic trip units (ComPacT NSX circuit breakers) |
|---|---|---|---|
|
66 / 115 |
344 |
57 |
156 |
|
127 / 220 |
180 |
29 |
81 |
|
230 / 400 |
99 |
16 |
44 |
|
347 / 600 |
66 |
10 |
29 |
|
400 / 690 |
57 |
23 |
26 |
|
1,000 |
39 |
16 |
0 |
General Rule: Power Supply Through the ULP Cord
Only one device can be powered through the ULP cord. This device must be at the end of the ULP line. It can be done only for the following devices:
-
FDM121 display.
-
BSCM module and MicroLogic trip unit for ComPacT NSX circuit breakers.
-
BSCM module for ComPacT NSX DC circuit breakers.
-
BCM ULP module for MasterPact NT/NW and ComPacT NS circuit breakers.
|
A |
IFE server |
|
B |
IFM interfaces stacked on IFE server |
|
C |
FDM121 display |
|
D |
IO module |
|
E |
MicroLogic trip unit in ComPacT NSX circuit breaker |
Length of ULP Cords
The rules for ULP cord length are as follows:
-
The maximum length of the ULP cord between two ULP modules in an IMU is 5 m (16.4 ft) if one of the ULP modules does not have an external power supply.
-
The maximum length of the ULP cord between two ULP modules in an IMU is 10 m (32.8 ft) if both ULP modules have an external power supply.
-
The maximum length of all the ULP cords on a single IMU is 20 m (65.6 ft).
-
In the case of an installation with a withdrawable drawer, the total length of the ULP cords for the fixed part must be less than 12 m (39.4 ft). This length limitation is to ensure that the fixed part operates correctly when the drawer is drawn out.
-
The bending radius of the ULP cords must be 50 mm (1.97 in) minimum.
-
A MasterPact MTZ circuit breaker and an IFE interface.
-
A MasterPact MTZ circuit breaker, one IO module, and an IFE interface.
-
A MasterPact MTZ circuit breaker, two IO modules, and an IFE interface.
Summary of Connection Rules
|
Characteristic |
Value |
|---|---|
|
Connection |
Daisy-chaining of ULP cords and ULP line termination at the end of the ULP line. |
|
Maximum length |
|
|
Voltage range supported |
24 Vdc -10%/+10% (21.6–26.4 Vdc) |
|
300 mA |