Hardware and Firmware Compatibility of ULP Modules
Introduction
ULP modules must be compatible with both the hardware and firmware.
The hardware and firmware compatibility of ULP modules can be checked with:
Hardware Compatibility
The following table lists the compatible ULP modules for each range of circuit breakers.
|
ULP module |
Part number |
Circuit breakers |
||
|---|---|---|---|---|
|
MasterPact MTZ with ULP port module and MicroLogic control unit |
MasterPact NT/NW or ComPacT NS with BCM ULP module and MicroLogic trip unit |
ComPacT NSX with BSCM module and/or MicroLogic trip unit |
||
|
IFE Ethernet interface for one circuit breaker |
LV434001 |
✓ |
✓ |
✓ |
|
IFE Ethernet switchboard server |
LV434002 |
✓ |
✓ |
✓ |
|
EIFE embedded Ethernet interface for one MasterPact MTZ drawout circuit breaker |
LV851001 |
✓ |
– |
– |
|
Spare part kit EIFE for one MasterPact MTZ1 drawout circuit breaker |
LV851100SP |
✓ |
– |
– |
|
Spare part kit EIFE for one MasterPact MTZ2/MTZ3 drawout circuit breaker |
LV851200SP |
✓ |
– |
– |
|
IFM Modbus-SL interface for one circuit breaker with Modbus-SL RJ45 port |
LV434000 |
✓ |
✓ |
✓ |
|
IFM Modbus-SL interface for one circuit breaker with Modbus-SL 5-pin connector |
TRV00210 |
– |
✓ |
✓ |
|
FDM121 front display module for one circuit breaker |
TRV00121 |
✓ |
✓ |
✓ |
|
IO input/output application module for one circuit breaker |
LV434063 |
✓ |
✓ |
✓ |
|
Service Interface |
LV485500 |
– |
✓ |
✓ |
|
USB maintenance interface |
TRV00911 |
– |
✓ |
✓ |
Firmware Compatibility Matrix
The primary reason for updating the system is to obtain the latest system features. The latest device firmware baseline and version details of the devices are available in EcoStruxure Power Commission software.
Checking Hardware and Firmware Compatibility with ULP Status LED
The yellow ULP LED indicates the mode of the ULP module.
|
ULP LED |
Mode |
Action |
|---|---|---|
|
Nominal |
None |
|
|
Conflict |
Remove extra ULP module |
|
|
Degraded |
Replace ULP module at the next maintenance operation |
|
|
Test |
None |
|
|
Non-critical firmware discrepancy |
Update firmware at the next maintenance operation |
|
|
Non-critical hardware discrepancy |
Replace ULP module at the next maintenance operation |
|
|
Configuration discrepancy |
Install missing features |
|
|
Critical firmware discrepancy |
Use EcoStruxure Power Commission software to check the firmware and hardware compatibility and follow the recommended actions |
|
|
Critical hardware discrepancy |
||
|
Stop |
Replace ULP module |
|
|
Power off |
Check power supply |
Checking Hardware and Firmware Compatibility with EcoStruxure Power Commission Software
EcoStruxure Power Commission software can be used to check hardware and firmware compatibility of the modules in the IMU and to get recommended actions to recover from a compatibility discrepancy situation.
For more information, refer to EcoStruxure Power Commission Online Help.