IFM Interface with Part Number TRV00210
Introduction
The IFM interface with part number TRV00210 is substituted by the IFM interface with part number LV434000.
The following table shows the specificities for each IFM interface.
|
Characteristics |
IFM interface TRV00210 |
IFM interface LV434000 |
|---|---|---|
|
Circuit breaker compatibility |
|
|
|
Modbus connector |
5-pin |
RJ45 |
|
Cable |
Free-ends Modbus cable |
RJ45 Modbus cables |
|
Modbus circuit |
D0, D1, common C, power supply |
D0, D1, 0 VL common |
|
Connection of the 0 V common to a ground terminal block |
Yes, ground terminal block required. |
No, given that 0 VL is isolated. |
|
Modbus isolation |
Two-wire RS 485 isolated repeater required |
No repeater required |
|
Modbus line termination |
Screwed |
RJ45 |
The specific features of IFM interface with part number TRV00210 , including rules for ULP connection and power supply, are detailed in this appendix.
Hardware Description
|
A |
5-pin screw type connector (Modbus connection and power supply) |
|
B |
Modbus address rotary switches |
|
C |
Modbus traffic LED |
|
D |
Modbus locking pad |
|
E |
ULP LED |
|
F |
Test button |
|
G |
Mechanical lock |
|
H |
Two RJ45 ULP ports |
|
I |
Stacking accessory |