DOCA0093EN-05

Compatibility Check of Device/Firmware and Corrective Actions

Overview

When ULP modules are upgraded with new functionalities, verify with the EcoStruxure Power Commission software that they are compatible with the different modules in the IMU system. Use the Firmware Upgrade table to perform diagnostics and identify discrepancies between the ULP modules. This table also provides the recommended actions relevant to the detected discrepancies.

NOTE: Compatibility check will only work if the device is connected.

Firmware Upgrade

To view the firmware status, click Firmware in the Device view.

The Firmware Upgrade window displays the following compatibility table.

Legend

Name

Description

A

IP address

Displays the IP address of the connected device.

B

Modbus address

Displays the Modbus address of the connected device.

C

Module

Lists the ULP modules of the connected device.

D

Status

Displays the compatibility status of the module inside the system.

E

Device Version

Displays the current firmware version installed in the module.

F

Available Version

Displays the latest firmware version available for upgrade.

G

Recommended Action

Provides the solution for discrepancies.

H

Refresh

Updates the changes made as per the recommended action.

Status

The Status column identifies the discrepancy conditions within the ULP modules.

Icons

Module status

Nominal

Non-critical firmware discrepancy

Or

Non-critical hardware discrepancy

Critical firmware discrepancy

Critical hardware discrepancy

Or

Hardware degraded

Stop

Or

Conflict

Recommended Actions

The Recommended Action column on the Firmware Upgrade window provides a solution to resolve a discrepancy. Each discrepancy has a generic predefined recommended action.

The table lists the recommended actions to take in the case of a detected discrepancy.

Module status

Description

Recommended action

Nominal

The ULP module is in nominal mode.

None.

Non-critical firmware discrepancy

There is a non-critical firmware discrepancy between the ULP module and other modules in the IMU.

Upgrade firmware at the next maintenance operation.

Non-critical hardware discrepancy

There is a non-critical hardware discrepancy between the ULP module and other modules in the IMU.

Replace module at the next maintenance operation.

Critical firmware discrepancy

There is a critical firmware discrepancy between the ULP module and other modules in the IMU.

Upgrade firmware.

Critical hardware discrepancy

There is a critical hardware discrepancy between the ULP module and other modules in the IMU.

Replace module.

Hardware degraded

The ULP module is in degraded mode.

Replace module at the next maintenance operation.

Stop

The ULP module is out of service.

Replace module.

Conflict

The ULP module is in conflict mode.

Remove duplicate module.

Refresh

After performing a recommended action for a specific discrepancy, you can click the Refresh button to update the changes in the Firmware Upgrade window.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?