ULP System Presentation
Description
Use the ULP (Universal Logic Plug) system to construct an electrical distribution solution which integrates metering, communication, and operating assistance functions for circuit breakers.
|
Legend |
Description |
Part of the ULP system |
|---|---|---|
|
A |
FDM128 Ethernet display for eight devices |
– |
|
B |
FDM121 front display module for one circuit breaker |
✔ |
|
C |
IFE Ethernet interface for one circuit breaker |
✔ |
|
D |
IFE Ethernet switchboard server |
✔ |
|
E |
IFM Modbus-SL interface for one circuit breaker |
✔ |
|
F |
IO input/output application module for one circuit breaker |
✔ |
|
G |
MasterPact MTZ drawout circuit breaker |
✔ |
|
H |
MasterPact MTZ fixed circuit breaker |
✔ |
|
I |
MasterPact NT/NW circuit breaker |
✔ |
|
J |
ComPacT NS circuit breaker |
✔ |
|
K |
ComPacT NSX circuit breaker |
✔ |
|
L |
ULP port module for MasterPact MTZ circuit breakers |
✔ |
|
M |
EIFE embedded Ethernet interface for one MasterPact MTZ drawout circuit breaker |
✔ |
|
N |
ULP line termination |
✔ |
|
O |
RJ45 plug/plug ULP cord |
✔ |
|
P |
Circuit breaker BCM ULP cord |
✔ |
|
Q |
NSX cord |
✔ |
|
R |
Ethernet switch |
– |
|
S |
Panel server |
– |
|
T |
BCM ULP circuit breaker communication module |
✔ |
|
U |
Cord between ULP port module and EIFE interface |
✔ |
|
V |
MicroLogic X control unit for MasterPact MTZ circuit breakers |
✔ |
|
W |
MicroLogic trip unit for MasterPact NT/NW and ComPacT NS circuit breakers |
✔ |
|
X |
MicroLogic 5, 6, or 7 trip unit for ComPacT NSX circuit breakers |
✔ |
|
Y |
PC with EPC software for test and commissioning of the IMUs |
✔ |
Features
Use the ULP system to enhance the functions of ComPacT NSX , ComPacT NS , MasterPact NT/NW , and MasterPact MTZ circuit breakers by:
-
An Ethernet communication link for access and remote monitoring with the IFE interface or EIFE interface ( MasterPact MTZ drawout circuit breakers only).
-
Web access to monitor and control the circuit breaker connected to an IFE interface or EIFE interface ( MasterPact MTZ circuit breakers only).
-
An input/output application with an IO module. It benefits from the extended capability of the IO module to monitor and control position of drawout circuit breakers in the cradle, circuit breaker operation, and custom application, and so on.
-
Test, setup, and maintenance functions with EcoStruxure Power Commission software.
-
A Modbus-SL communication link for access and remote monitoring with the IFM interface.
-
Local display of measurements and operating assistance data with the FDM121 display.
The ULP system lets the circuit breakers become a metering and supervision tool to assist energy efficiency and can:
-
Optimize energy consumption by zone or by application, according to the load peaks or priority zones.
-
Improve electrical equipment management.
Intelligent Modular Unit (IMU)
A modular unit is a mechanical and electrical assembly containing one or more products to perform a function in electrical equipment (incoming protection, motor command, and control). The modular units are easily installed in the electrical equipment.
The circuit breaker with its internal communicating components (for example, MicroLogic ™ trip unit) and external ULP modules (for example, IO module) connected to one communication interface (IFM, IFE, or EIFE depending on the circuit breaker type) is called an IMU.
Examples of IMU with ComPacT NSX Circuit Breaker
|
A |
IFM Modbus-SL interface for one circuit breaker |
|
B |
NSX cord |
|
C |
NSX cord terminal block (included with NSX cord) |
|
D |
MicroLogic trip unit |
|
E |
BSCM circuit breaker status control module |
|
F |
RJ45 plug/plug ULP cord |
|
G |
ULP line termination |
|
H |
FDM121 front display module for one circuit breaker |
|
A |
IFE Ethernet interface for one circuit breaker |
|
B |
ULP line termination |
|
C |
RJ45 plug/plug ULP cord |
|
D |
NSX cord |
|
E |
CE/CD (connected/disconnected) position auxiliary switches |
|
F |
Support for two moving connectors |
|
G |
9-wire moving connector |
|
H |
9-wire fixed connector for base |
|
I |
IO input/output application module for one circuit breaker |
Examples of IMU with MasterPact NT/NW Circuit Breaker
|
A |
IFM Modbus-SL interface for one circuit breaker |
|
B |
Circuit breaker BCM ULP cord |
|
C |
Fixed terminal block |
|
D |
BCM ULP circuit breaker communication module |
|
E |
Fixed electrically-operated circuit breaker |
|
F |
RJ45 plug/plug ULP cord |
|
G |
ULP line termination |
|
H |
FDM121 front display module for one circuit breaker |
|
A |
IFE Ethernet interface for one circuit breaker or IFE Ethernet switchboard serve |
|
B |
ULP line termination |
|
C |
RJ45 plug/plug ULP cord |
|
D |
Circuit breaker BCM ULP cord |
|
E |
Circuit breaker disconnected position contact (CD) |
|
F |
Circuit breaker cradle |
|
G |
BCM ULP circuit breaker communication module |
|
H |
Drawout circuit breaker |
|
I |
Drawout terminal block |
|
J |
Circuit breaker connected position contact (CE) |
|
K |
Circuit breaker test position contact (CT) |
|
L |
IO input/output application module for one circuit breaker |
Examples of IMU with MasterPact MTZ Circuit Breaker
|
A |
IFE Ethernet interface for one circuit breaker or IFE Ethernet switchboard server |
|
B |
ULP line termination |
|
C |
IO input/output application module for one circuit breaker |
|
D |
RJ45 plug/plug ULP cord |
|
E |
ULP port module |
|
F |
MasterPact MTZ fixed circuit breaker |
|
A |
IO input/output application module for one circuit breaker |
|
B |
ULP line termination |
|
C |
ULP port module |
|
D |
RJ45 plug/plug ULP cord |
|
E |
MasterPact MTZ drawout circuit breaker |
|
F |
Cord between ULP port module and EIFE interface |
|
G |
EIFE embedded Ethernet interface for one MasterPact MTZ drawout circuit breaker |