Standalone Architecture
Introduction
When the intelligent modular units are not communicating to communication interfaces (IFE, EIFE, or IFM interfaces), the architecture is classified as standalone.
Standalone Architecture
The following figure shows an example of a standalone architecture with IMUs consisting of an FDM121 front display module for one circuit breaker or an IO input/output application module for one circuit breaker and a compatible circuit breaker equipped with a MicroLogic trip unit.
|
A |
IO module |
|
B |
24 Vdc AD power supply for MicroLogic trip units in MasterPact NT/NW or ComPacT NS circuit breakers |
|
C |
24 Vdc ABL8 power supply for ULP modules |
|
D |
Circuit breaker BCM ULP cord |
|
E |
NSX cord |
|
F |
FDM121 display |
|
G |
ULP line termination |
For FDM121 display mounting options,
refer to QGH80971,
Enerlin’X FDM121 - Front Display Module for One Circuit Breaker - Instruction Sheet
The 24 Vdc power supply is selected from the list of recommended 24 Vdc power supplies. The power supply rating must be selected according to IMU consumption.