Intelligent Modular Unit (IMU) with Withdrawable Drawer
Installation in a Withdrawable Drawer
In equipment with withdrawable drawers, the circuit breaker is found in the withdrawable drawer. The IFE or IFM interface and IO modules must always be in the fixed part.
Connection of the Withdrawable Drawer
The ULP connection between the fixed part and the part built into the withdrawable drawer is made with the pluggable control terminal blocks on the unit.
RJ45 Pin Connection of ULP Cord
The RJ45 plug/plug ULP cord uses an RJ45 connector with pin connection as follows:
Connection Procedure
The procedure for connecting the withdrawable drawer terminal block is as follows:
|
Step |
Action |
|
|---|---|---|
|
1 |
Plug the four conductors into the terminal block (removable side):
|
|
|
2 |
Plug the four ULP cord conductors into the terminal block on the fixed part in the same order. |
|
|
3 |
Strip the ULP cord insulation:
|
|
|
4 |
Insert the wire braid into a grounding clamp at both ends of the stripped ULP cord. |
|
|
5 |
Screw the grounding clamps on the fixed part and withdrawable part of the drawer. |
|