DUG_Multiwire Puck Dimmer_LK-02

Adjusting the brightness level using app

Using the , you can increase/decrease the brightness level remotely.
To increase/decrease the brightness level:
  1. On the Home page, tap All devices.
  2. In Dimmer Micromodule tap the power button (A) to turn on/off the device.

  3. Tap for slide-up menu.
  4. In the slide-up menu, drag the sliding bar (B) to increase/decrease the brightness.

  5. Alternatively, you can navigate to device menu and tap on (C) to turn on/off the device. When the device is turned on, drag the sliding bar (D) up/down to increase/decrease the brightness.

    NOTE: Some lamps have a starting point. When you turn on the lamp at a low brightness, it quickly gets very bright and then goes back to the lower brightness automatically. This is the behaviour of the lamp and the dimmer can't change it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?