DUG_Multiwire Puck Dimmer_LK-02

Push button moment control

A Moment allows you to group multiple actions that are usually performed together. Using the app, you can create moments based on your needs (such as movie night) and configure them to the Wireless Switch push buttons.

Creating a moment for push button

  1. Select Moment Control in the slide-up menu.

  2. Select Moment 1 or Moment 2

    NOTE:
    • Short press the push button to trigger the Moment 1.

    • Long press the push button to trigger the Moment 2.

  3. On Moment page tap + to create a new moment.

  4. Tap Edit name , enter the moment name (A) and tap Save.

    TIP: You can choose the cover image that represents your moment by tapping .

  5. In the Action section, tap Add task to open the slide-up menu.

  6. Select the dimmers which you want to add in the moment and tap Next.

    TIP: You can add one or more actions using .

  7. Tap Save to verify and save the moment.

Assigning moment to push button

In Moment Control page, tap on the moment to save the to save the settings.

Editing a push button moment

  1. In Moment Control page, locate the moment you want to edit and tap .

  2. On the Edit page, you can tap each item to change the settings and tap Save.

    TIP:
    • You can add one or more actions using .

    • To delete an existing action, slide each item towards left and tap Delete.

Unbinding a moment from Push button

  1. In Moment Control page, tap on the moment you want to unbind.

  2. Tap Unbind to remove the moment assigned to a push button setting.

Deleting a lighting moment

  1. In Moment Control page, locate the moment you want to delete and tap .

  2. Tap Delete.

    NOTE: Deleting a moment will unbind the moment from push button setting.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?