DUG_Multiwire Puck Dimmer_LK-02

Local control

You can set the push button switch action to control the load locally.
  1. Select Local Control in the slide-up menu.
  2. Select one of the option based on your requirement:
    • Turn On, Dim Up
    • Turn Off, Dim Down
    • Turn On/Off, Dim Up/Down
    NOTE:
    • Turn on/off will be assigned to short press..

    • Dimming up/down will be assigned to long press

    IMPORTANT:
    • If you have configured a push button with the Turn On, Dim Up option, you can use it to both turn on the light and increase its brightness. However, to turn off the light and reduce its brightness, you should configure another push button with the Turn Off, Dim Down option, or you can perform these actions using the app.

    • If you have configured a push button with the Turn Off, Dim Down option, you can use it to both turn off the light and decrease its brightness. However, to turn on the light and increase its brightness, you should configure another push button with the Turn On, Dim Up option, or you can perform these actions using the app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?