DUG_Multiwire Puck Dimmer_LK-02

Example of an automation

This demonstration shows you how to create an automation to turn on the dimmer at the scheduled time.
  1. Go to Automation > + to create an automation.
  2. Tap Edit name, enter the name of the automation and tap Save.
    TIP: You can choose the cover image that best represents your automation by tapping .
  3. Tap Add Condition > Schedule.
    • Tap Repeat (A), select the days you want to set the schedule and tap Save.

    • Set the time (B) at which the automation must start and tap Next.

  4. Tap Add task > Run the device > Dimmer Micromodule.
  5. Tap Dimmer (C) and in the slide-up menu, select On and tap Save.
  6. Tap Brightness (D) and update the required brightness level and tap Save.

  7. Tap Next.
  8. In the Automation Settings page, tap Save.

    Once the automation is saved, it is visible on the Automation tab. You can tap the toggle switch on the automation to enable it.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?