DUG_Multiwire Puck Dimmer_LK-02

Operating a Dimmer

You can switch the dimmer ON/OFF and adjust its brightness using the paired Wireless switch.
  • Short press the left or right of the Wireless switch (< 0,5 s) to turn ON/OFF the connected load (A).

  • Long press the left or right of the Wireless switch (> 0,5 s) to increase or decrease the brightness of the connected load (B).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?