DUG_Multiwire Puck Dimmer_LK-02

Checking the type of wiring mode

Using the Wiser app, you can check whether the dimmer is connected with or without neutral wire.
  1. On the Home page, tap All devices > Dimmer Micromodule.
  2. Tap and tap Device information.
    You see the type of wiring mode (A) in the app.

    NOTE: Virtual ID and MAC address may vary with the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?