DUG_Multiwire Puck Dimmer_LK-02

Dimmer settings

Using the app, you can manage the Dimmer modes and settings.

To access the dimmer settings:

  1. On the Home page, tap All devices > Dimmer Micromodule.

  2. On the device control panel page, tap Settings.

Dimming mode

You can change the dimming mode in the app if you have problems with light flickering. This improves the dimming quality.

Tap Dimming Mode (A) and select either of the following:

RC - When load is connected to the dimmer.

Leading Edge - When a LED is connected to the dimmer. Only choose this mode if the LED is not working properly in RC mode.

NOTE: Leading Edge mode uses 10 % of the nominal load to avoid overheating of the Dimmer, refer to technical data.

Dimming range

You can restrict the maximum and minimum brightness of the load connected to the device. This is done to avoid flickering and switching off the LED.

Tap Dimming Range (B) and do either or both of the following:

Min Brightness - Drag the sliding bar to restrict the minimum brightness.

NOTE: When you slide the bar to the right to set the minimum brightness, the light maintains the minimum brightness level, even if you drag the sliding bar to the lowest value in the control panel.

Max Brightness - Drag the sliding bar to restrict the maximum brightness.

NOTE: When you slide the bar to the left to set the maximum brightness, the light maintains the maximum brightness level, even if you drag the sliding bar to the highest value in the control panel.

TIP: You can also adjust the dimming range by pressing the +/- buttons below the sliding bar.

Toggle mode setting

Using this setting, the device will remember the last state of the device.

Tap Toggle Mode Setting (C) and select any one of the following:

100% - The LED glows at maximum brightness every time it is turned on.

Last Level (Memory Function) - The LED glows at the previously set brightness level whenever it is turned on.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?