DUG_Multiwire Puck Dimmer_LK-02

Adjusting the brightness on the dimmer

You can set the minimum/maximum brightness of the dimmer.

IMPORTANT: Set the minimum/maximum brightness settings of the dimmer only after pairing it with Wireless switch. Refer Pairing Wireless switch with Multiwire micro module dimmer.

Press and hold the left mechanical push button for 15 s.

The dimmer LED blinks green and then the connected load blinks till the settings mode is confirmed.

Refer to the following sections for minimum and maximum brightness settings.

NOTE: Some lamps have a starting point. When you turn on the lamp at a low brightness, it quickly gets very bright and then goes back to the lower brightness automatically. This is the behaviour of the lamp and the dimmer can't change it.

Adjusting minimum brightness:

  1. When in brightness settings mode, short press the left mechanical push button 2 times.

    The light reaches the minimum brightness level.

  2. Long press the left mechanical push button to set the minimum brightness of your choice.

    TIP: If you release the push button and then long press it again, it will adjust the brightness in the opposite direction from the previous dimming action (either darker or brighter, based on the prior dimming direction).

  3. Wait for the time out for 30 s or short press the left mechanical push button 2 times to confirm the settings.

    The light blinks for few times indicating that the setting is saved.

Adjusting maximum brightness:

  1. When in brightness setting mode, short press the left mechanical push button 4 times.

    The light reaches current maximum brightness level.

  2. Long press the left mechanical push button to set the maximum brightness of your choice.

    TIP: If you release the push button and then long press it again, it will adjust the brightness in the opposite direction from the previous dimming action (either darker or brighter, based on the prior dimming direction).

  3. Wait for the time out for 30 s or short press the left mechanical push button 2 times to confirm the settings.

    The light blinks for few times indicating that the setting is saved.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?