DUG_Multiwire Puck Dimmer_LK-02

Group control

A group allows you to trigger set of device action at the same time that are usually performed together. Using the app, you can create group based on your needs (such as bed time).

Creating a group

  1. Select Group Control in the slide-up menu and then tap + to create a new group.

  2. Tap Edit name , enter the group name (A) and tap Save.

    TIP: You can choose the cover image that represents your group by tapping .

  3. In the Action section, tap Add task to open the slide-up menu.

  4. Select the dimmers which you want to add in the group and tap Next.

    TIP: You can add one or more actions using .

  5. Tap Save to verify and save the group.

Adding a group

In Group Control page, tap on the group to save the to save the settings.

Editing a group

  1. In Group Control page, locate the group you want to edit and tap .

  2. On the Edit page, you can tap each item to change the settings and tap Save.

    TIP:
    • You can add one or more actions using .

    • To delete an existing action, slide each item towards left and tap Delete.

Unbinding a group

  1. In Group Control page, tap on the group you want to unbind.

  2. Tap Unbind to remove the group assigned to a push button setting.

Deleting a lighting group

  1. In Group Control page, locate the group you want to delete and tap .

  2. Tap Delete.

    NOTE: Deleting a group will unbind the group from push button setting.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?