DUG_Multiwire Puck Dimmer_LK-02

Push button control

Using the app, you can configure the Push Button to control devices connected locally and also to remotely control a moment or a group.

To access push button control settings:

  1. On the Home page, tap All devices > Dimmer Micromodule.

  2. On the device control panel page, tap Settings.

  3. Select the push button which you want to configure.

    - Push Button 1

    - Push Button 2

  4. On the slide-up menu select any one of the following:

    - Group Control

    - Moment

    - Local Control

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?