DUG_Multiwire Puck Dimmer_LK-02

Resetting the device

You can reset the device to factory default manually.
  1. Short press the Set (Setup/Reset) button 3 times (< 0.5 s) and then long press the Set (Setup/Reset) button once (>10 s).
    or
    Short press the mechanical push button-1 for 3 times and then long press the push button once for 10 s.

  2. After 10 s, LED starts blinking red, then release the push-button.
    NOTE: All configuration data, user data, and network data are deleted.
      The LED stops blinking upon successful reset of the device.
      The device restarts and blinks green for a few seconds.
    QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

    Was this helpful?