DUG_Aidoo Pro Heat Pump_WH-00

About Aidoo Pro Wi-Fi® and Wiser System

Airzone specializes in HVAC (Heating, Ventilation, and Air Conditioning) control solutions. Aidoo Pro Wi-Fi® (hereafter referred to as Aidoo) allows you to control your air to water Heat Pump using the Wiser Home app.

Beta Feature:

  • Provided as‑is. Fully functional but not final for commercial release. No assurances of performance apply. Limited technical support is available, with no commitment to issue resolution. Use at your own risk.
    Your feedback is highly valued, please do not hesitate to share your experience with our customer care, as it will help improve the quality and maturity of this solution.

  • The Airzone Air to Water solution is applicable for customers in France and United Kingdom.

To monitor and control the heating system with the Aidoo, you need a Wiser Hub or HubR and one of the following Wiser temperature control devices:

  • Wiser room thermostat

  • Wiser temperature and humidity sensor

  • Wiser radiator thermostat

  • Wiser connected flush mounted thermostat

  • Wiser Under-floor heating strip

NOTE: Availability of these devices may vary as per the country.

Advantages of Aidoo Pro Air to Water and Wiser System:

  • Seamless Communication

    Interfaces with the Heat Pump using the manufacturer's protocol.

  • Remote Control

    Offers an easy-to-use interface for remote control of the Heat Pump via the Wiser Home app.

  • Optimal Performance

    Ensures the Heat Pump operates normally while maintaining its functionality and efficiency.

  • Manage Heating and Hot Water

    • Room Temperature Regulation: Adjust the temperature in each room (when applicable) using the Wiser Home app in conjunction with Wiser climate control devices like thermostats or temperature sensors. The app displays the current temperature, set point, and status of each heating zone.

    • Comprehensive Control: Manage home heating by creating, editing, and managing schedules and modes such as Eco, Comfort, and Away.

    • Hot Water Management: Easily create schedules and boost domestic hot water using the Wiser Home app.

  • Enhanced Energy Management

    • Energy Consumption Visualization: Monitor energy usage by integrating a Schneider PowerTag E (wireless energy sensor).

      NOTE: Availability of Schneider PowerTag E may vary as per the country.
    • Optimized Energy Use: Adapt energy consumption to align with energy tariffs for better efficiency.

  • Fault Visualization

    Provides clear visualization of any faults detected in the Heat Pump.

Aidoo Pro Air to Water wired connection

Aidoo is wired directly to the Heat Pump and connects to the Wiser Home app via Wi-Fi, allowing you to control the air to water Heat Pump using the app.

The wired connection between Aidoo and the Heat Pump ensures:

  • Reliable Control: guarantees consistent and dependable control of the Heat Pump.

  • Communication Failures: eliminates communication failures and unintended activations.

  • Manufacturer Validation: ensures communication with the Heat Pump is validated by the manufacturer.

IMPORTANT: A 2.5 meters cable is provided with the Aidoo to connect it with the Heat Pump. If the distance between the Aidoo and the Heat Pump is more, you can use spare cables of 2.5 meters. However, the maximum length limitation of the cables is 10 meters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.