DUG_Aidoo Pro Heat Pump_WH-00

Configuring the Panasonic Aquarea Heat Pump

The Panasonic Aquarea Heat Pump supports several operating modes that determine how heating and domestic hot water are controlled. These modes must be configured on the Panasonic controller before using it with Wiser. Following are the Heat Pump recommended configurations that can be set on the Panasonic Aquarea Heat Pump:

Installer Setup > System setup > Zone & Sensor

  • Leaving water temperature

  • Ambient room:

    • External: Heat Pump operates based on the external temperature.

    • Internal: Heat Pump operates based on the internal room temperature.

Alternative configuration options

Panasonic Aquarea also supports the following (less recommended) modes:

  • Room Mode

  • Weather Compensation Curve (Water temperature is adjusted automatically based on the outdoor temperature)

  • Fixed Circulation Water Temperature (Water temperature is maintained at a constant value)

DHW (Domestic Hot Water) modes

The table below clarifies how DHW behaves when controlled through Aidoo and Wiser.

DHW Mode ON/OFF Behavior (via Wiser/Aidoo) Set Point Behavior (Wiser/Aidoo) Additional Notes
ON/OFF The ON/OFF button in the app enables or disables DHW. DHW heats until the set point is reached​.
The set point can be changed from the Panasonic controller.
ON = heat to set point, ​ ​
OFF = stop.​
Set point The ON/OFF button in the app activates/de–activates DHW operation.
The set point can be changed using the Aidoo app.
Whenever a new command is set in the app, it overrides the previous settings. So, the most recent signal always takes the priority​.
The ON/OFF button in the app activates/de–activates DHW operation.
You can change the original set point using the Wiser Home app.
Whenever a new command is sent from the app, it overrides any previous settings - the most recent signal always takes priority​.
Temperature and timing are managed by the latest command sent either from the Panasonic controller, Airzone app or the Wiser Home app.
Scheduled ​ (ON/OFF + Set point) The ON/OFF button in the app activates/de–activates DHW operation.
If set to OFF, DHW is inactive.
If set to ON, it follows the schedule set in the Heat Pump.
You can change the original set point and customize your schedule using the Wiser Home app.
Whenever a new command is sent from the app, it overrides any previous settings — the most recent signal always takes priority​.
The ON/OFF and set point are managed by the latest command sent either from the Panasonic controller, Airzone app or the Wiser Home app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.