DUG_Aidoo Pro Heat Pump_WH-00

Setting the maximum hot water temperature

The hot water is the water used for sanitary needs like showers and cleaning. It is not the water used for space heating in radiators or underfloor heating.

To prevent bacterial growth in the hot water tank and reduce the risk of Legionnaires disease, follow the guidance from your Heat Pump manufacturer.

TIP: Save on costs by ensuring that your hot water is operating during a low tariff period.

To set the maximum hot water temperature:
  1. On the Control tab, tap All devices or a room tab where the Aidoo Pro Heat Pump is located and tap Heat Pump > Device settings.
  2. Tap (A) and set the maximum hot water temperature.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.