DUG_Aidoo Pro Heat Pump_WH-00

Operating the hot water tank

Using the Wiser Home app, you can turn on/off the hot water tank and activate the boost mode for a time span.
The boost mode will override the scheduled operation of the hot water tank.

The Hot Water controls in the app will take over domestic hot water (DHW) control through Aidoo. This control is active, until the Aidoo is disconnected from the hub.

The below icons indicate the on/off status of the hot water tank:
Icon Hot water tank – Status
OFF
ON

To turn on/off the hot water tank:
  1. On the Control tab, select Hot Water (A).
  2. Tap (B) to turn the hot water tank on/off.
  3. Tap and set the duration to activate the boost mode.
    NOTE: In case there is a immediate need for domestic hot water, there is a possibility to boost its production. Boost will then trigger direct electrical heating which is less efficient than heat pumping but is much quicker. Boost mode can be deactivated by tapping and selecting Off.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.