DUG_Aidoo Pro Heat Pump_WH-00

Managing a schedule for temperature control

The temperature can be controlled and triggered by a schedule. You can create/edit the schedules at any time. A default heating schedule appears, you can keep this schedule or change it as needed.

Using the Wiser Home app, you can manage schedules for:
  • a room

  • hot water tank.

NOTE: When the schedule begins, you can see the until time on the Control tab under the device name. The until time indicates how long the device will remain in its current state according to the schedule.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.