DUG_Aidoo Pro Heat Pump_WH-00

Managing heating schedule for a room

You can create a new schedule or manage the events of a schedule to adjust the room temperature.

To manage a schedule:
  1. On the Home screen, tap > Schedules > .
  2. Enter a NAME for the schedule (A) and select the list of rooms (B) where the schedule must apply.
    NOTE:
    • The TYPE (Climate) and TEMPERATURE CONTROL (Heating) fields cannot be changed.

    • Wiser with Aidoo can operate in heating mode not in cooling mode.

  3. Tap Create.
  4. Tap See my schedule.
    NOTE: A set of default events are created for the new schedule.
  5. Select the day (C), for which you want to add an event.
  6. Tap (D) to add an event.
    1. Set the TEMPERATURE (E).
    2. Select WHEN (F) to set the time for activation of the event.
  7. Tap Set.
    TIP:
    • You can tap corresponding to an event and modify the event.

    • You can add multiple events in a schedule based on your requirement by following the steps 5 to 7.

    • You can tap to copy all the events from:

      • one day to other days.

      • one schedule to another schedule.

    NOTE: If the room temperature is set manually, an ongoing event is overridden by the manual setting.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.