DUG_Aidoo Pro Heat Pump_WH-00

Configuring the Daikin Altherma 3 Heat Pump

The Daikin Altherma 3 Heat Pump supports several operating modes that determine how heating and domestic hot water are controlled. These modes must be set correctly for Wiser to control heating effectively.

Recommended Configuration (Daikin Controller):

  • Installer settings > Overview field settings > C – 07:

    • 0 – Leaving Water Temperature (LWT) Mode

    • 2 – Ambient Room (AR) Temperature Mode

  • Installer settings > Overview field settings > 6 – 0D:

    • 0 – Reheat only

  • The Setpoint mode control configuration parameter must be set to Fixed. This is usually the default setting.

IMPORTANT: When using the Ambient Room (AR) mode, set the thermostat to the preferred highest temperature to allow Wiser to manage the heating effectively.

Alternative configuration options

Daikin also supports the following (less recommended) modes:

  Fixed – LWT (Leaving Water Temperature) Mode Weather Compensation - LWT Mode Fixed - Ambient Room Temperature Mode Weather Compensation - Ambient Room Temperature Mode
Set Point Mode: Fixed Weather Compensation Fixed Weather Compensation
Control Type: Leaving water temperature (LWT) Leaving water temperature (LWT) Ambient Room (AR) Ambient Room (AR)
Target Water Temperature: LWT setpoint Calculated by the heating curve Leaving water temperature (LWT) Calculated by the heating curve
Thermostat Control: LWT setpoint +/- Curve offset Room set point for demand Room set point for demand

Daikin Domestic Hot Water (DHW) Modes

DHW Mode ON/OFF Behavior (via Wiser/Aidoo) Set Point Behavior (Wiser/Aidoo) Additional Notes
Reheating Mode The ON/OFF button in the app activates/de–activates DHW operation. The set point selected in the Wiser Home app is applied.
DHW heats until the set point is reached.
ON = heat to set point
OFF = stop.
Scheduled Mode The ON/OFF button in the app activates/de–activates DHW operation.
If set to OFF, DHW is always off regardless of schedule.
The Wiser Home app set point is ignored. The system follows Daikin’s internal schedule (Comfort/Eco/Stop).
If OFF, DHW is always off regardless the schedule
Temperature and timing are managed by Daikin’s internal controller.
Scheduled + Reheating Mode The ON/OFF button in the app activates/de–activates DHW operation.
If set to OFF, DHW is inactive.
If set to ON, it follows the internal schedule set in the Heat Pump.
The Wiser Home app set point is not applied.
System follows Daikin’s schedule and logic.
If set to OFF, DHW is always OFF, regardless the schedule.
Reheating logic is overridden by the scheduling mode.

NOTE:
  • In Scheduled or Scheduled + Reheating mode, if DHW is ON, any set point change from app stays active only until the next scheduled period begins. After that, the system will follow the schedule set in Daikin’s controller.

  • Sometimes, the Daikin Onecta Cloud may get deactivated when the Heat Pump is re-powered. For seamless operation, check that the Onecta Cloud is active and reconnect it if necessary. This can be verified either via the system display or through the Daikin Onecta app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.