DUG_Aidoo Pro Heat Pump_WH-00

Managing the channel

You need to allocate a heating channel to any room that requires heating. The heating channel defines which heating source is used for that room.

To select the channel:
  1. On the Control tab, choose the required room.
  2. Tap > Room settings (A).
  3. Tap Channel (B).
  4. Select the required channel(s) out of the following:
    • Selecting 1 Channel – Standard Installation

      Virtual Channel – Heat Pump uses the Virtual Channel Heat Pump

      • When the home uses a single heating architecture, where rooms are heated directly by the Heat Pump, and no motorised valve needs to be controlled.

      • In this setup, assign the Virtual Channel Heat Pump to every room that requires heating.

      • Selecting this channel ensures the Heat Pump acts as the heating source for those rooms.

      • Make sure the Aidoo is commissioned first. The channel will not be visible until commissioning is complete.

      • If a room also uses a motorised valve (for example, radiators in mixed systems), follow the instructions in the Selecting 2 Channels section.

    • Selecting 2 Channels – Managing Architectures with a Motorised Valve

      IMPORTANT: The second channel is currently in beta testing and may cause some limitations. For standard installations, we recommend using only one channel per room.

      In a two zone architecture, where some radiators need to be controlled by a motorised valve, you do need to allocate two heating channels to those rooms:

      • Channel 1 or Channel 3 to control the motorised valve for the radiator zone.

      • Virtual Channel Heat Pump to call for heat from the Heat Pump.

      This ensures coordination between the heating zones so that:

      • UFH and radiators can operate independently.

      • The Heat Pump supplies heat when either zone calls for it.

    • None - You can select this option, if the room does not need to be heated.

    NOTE: If you have a Wiser HubR 1 channel, you will only see channel 1. If you have a Wiser HubR 3 channel, you will see channels 1 and 3.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.