DUG_Aidoo Pro Heat Pump_WH-00

Managing a schedule for the hot water tank

You can manage the events of a schedule for the hot water tank.

To manage a schedule:
  1. On the Control tab, select Hot Water > Edit Schedule.
  2. Select the day (A), for which you want to add an event.
  3. Tap (B) to add an event.
    1. Set the STATE (C) to turn the event On or Off.
    2. Select WHEN (D) to set the time for activation of the event.
  4. Tap Set.
    TIP:
    • You can tap corresponding to an event and modify the event.

    • You can add multiple events based on your requirement by following the steps 2 to 4.

    • You can tap to copy all the events from:

      • one day to other days.

      • one schedule to another schedule.


    NOTE: Instances when the ongoing events are overridden:
    • If the hot water tank is turned on/off manually.

    • When the boost mode is on, events are overridden until the boost mode is turned off.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.