DUG_Aidoo Pro Heat Pump_WH-00

Adjusting the room temperature

Using the Wiser Home app, you can adjust the room temperature.

NOTE: If a room is installed only with a radiator valve (ITRV) and the associated Heat Pump at home is set for cooling mode, the room temperature can not be adjusted.
However, the current temperature is still displayed for monitoring.

To adjust the room temperature:
  1. On the Control tab, select a room (A).
  2. Drag the slider (B) up/down to adjust the room temperature.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.