DUG_ARGUS Motion Sensor Outdoor 360_WH-03

Using the device in Quick Home Connect

When motion is detected within the sensor’s detection range, it will switch on the connected load (light) automatically. The light will remain ON for the duration specified in the time setting. For more information refer to Device settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?