DUG_ARGUS Motion Sensor Outdoor 360_WH-03

Device settings

You can adjust settings like sensitivity, time, LUX level of the motion sensor using a screwdriver.

Time setting

Time setting: Adjusts the duration for which the sensor activates or triggers the connected load after detecting motion.

NOTE: If you re-trigger the sensor, the timer will get reset. You can also change the status of the load before the set time expires. For more details on controlling the load's behavior, refer to Override modes.
Short Pulse : Load is switched ON for 1.5 s to trigger certain switches, e.g. to trigger timer for staircase lights.
NOTE: Short Pulse can only be triggered every 10 s.
5s - 1hr (Logarithmic scale): Set the duration for which the connected load stays ON after motion is detected. When time expires, the connected load will turn off automatically.
Test: Test the sensitivity setting. The Load turns ON for 2 s each time a motion is detected. The brightness setting will be ignored.
NOTE: Test can only be triggered every 5 s.

LUX setting LUX setting: Sets the ambient brightness threshold at which the sensor activates or triggers the connected load. When set to a specific lux level, the sensor will initiate its operation when the ambient brightness falls below the threshold level.
1-2000 Lux : Set the brightness threshold at which the sensor should turn ON the load. When the ambient brightness falls below the set lux level, the motion sensor will be triggered to operate.
Day mode : The sensor will turn the load ON if motion is detected, regardless of ambient brightness. This means that the sensor will respond to motion and trigger actions during both day and night.
Teach in Threshold : This setting allows the sensor to learn and save the current ambient brightness as the threshold for triggering the load.
When this setting is selected, the current ambient brightness will be saved as the threshold after 15 seconds, giving time for the installer to step back and capture the correct brightness. The sensor will then use this saved brightness level as a reference for triggering the load.

Sensitivity

Determines the detection range by adjusting the sensor's sensitivity level. The higher the sensitivity, the more the detection range.
Sensitivity level: 50%, 60%, 70%, 80%, 90%, 100%

Setup/Reset
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?