DUG_ARGUS Motion Sensor Outdoor 360_WH-03

Pairing the device with the Wiser Hub

Pre-requisite:
  • The motion sensor should be correctly wired and powered.

  • Control panel of the motion sensor should be accessible.


To pair the motion sensor:
  1. On the Home screen, tap .
  2. Tap Devices > > Safety and Security > Outdoor Motion Sensor.
    TIP: You can also navigate by tapping Control tab > > Safety and Security > Outdoor Motion Sensor.
  3. Tap Scan QR code and allow the Wiser Home app to access your camera. Then, scan the QR code located on the device.
    NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.

    If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:

    • (A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI-64 and Install code are valid.

    • (B): Tap this option if you are unable to find the Mac Address/EUI-64 and Install code.

  4. Tap Next and press the S/R button on the motion sensor three times. This starts the Joining process.
    The app confirms that the device is joined and a yellow LED blinks on the motion sensor.
  5. Mount the motion sensor on the wall or ceiling and tap Next to start configuring the motion sensor.

  6. Enter the name of the motion sensor and tap Next.
  7. Assign a location for the motion sensor from the list (C) and tap Next.
    TIP: If the location of the motion sensor is not there in the list (C), it can be added to the list by entering its name in the New room name box.
  8. Select a device from the list (D) that shall operate after motion detection and tap Next.
    NOTE: There are default settings for Sensitivity, Motion Detection Timer, Lux Level and motion detection notification. You can update them if necessary.
  9. Tap Finish.

    After you pair the device, a success screen appears with the following options:

    • + Add New Device: Tap to continue pairing more devices.

    • Start Using Your Device: Tap to start using the paired device.

    NOTE: The success screen appears only if you are logged in as a Home Owner.

The motion sensor is now listed on the Control tab under the All section and in the room it is assigned to.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?