DUG_ARGUS Motion Sensor Outdoor 360_WH-03

Resetting the device

You can reset the sensor to factory default manually.
To reset the sensor:

Short press the S/R (Setup/Reset) button 3 times (< 0.5 s) and then long press the S/R (Setup/Reset) button once (>10 s). After 10 s, LED starts blinking red. Release the button at this point.

Upon successfully resetting the sensor, the amber LED turns ON for 3 s and then turns OFF.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?