DUG_ARGUS Motion Sensor Outdoor 360_WH-03

Notification

Using the Wiser Home app, you can see the following notifications related to the operation of the motion sensor.
  1. Notification for motion detection: When you enable this notification, and the motion is detected by the motion sensor, you get the notifications in the app. To enable/disable this notification, refer to G of Configuring the motion sensor.

  2. Device off-line notification: You get this notification in the app when the motion sensor loses connectivity so you can restore the connectivity or troubleshoot the motion sensor at the earliest.

  3. Overheating notification: You get this notification in the app when the motion sensor is overheated after a prolonged operation.

NOTE: You can not enable/disable the device off-line and overheating notifications. The app displays the appropriate notification when the motion sensor overheats or goes offline.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?