DUG_ARGUS Motion Sensor Outdoor 360_WH-03

LED indications

Pairing the motion sensor with the Wiser Hub

User Action

Status

LED Indication

Press the S/R button of the motion sensor 3 times in quick succession.

When pairing is completed, LED blinks yellow.

LED blinks yellow.

Motion Detected

User Action

Status

LED Indication

When the motion is detected

The LED flashes red.

Resetting the Device

User Action

Status

LED Indication

Press the S/R (Setup/Reset) button 3 times within 0.5 seconds and then hold for 10 seconds

The red LED blinks for 10 seconds, flashes amber for 3 seconds, and then turns off.

→ (10 sec) → (3 sec)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?